Product Usage

Types of shafts in mechanical engineering - Linear shafts, rotating shafts, rods, and how to make the right choice

Shafts are a critical component of the mechanical engineering industry, as they connect various components. There are several types of shafts used in mechanical engineering, including linear shafts, rotary shafts, and rods. When selecting a shaft for a specific application, you must consider various factors to find the best shaft. These include the type of application, the performance requirements, and the type of shaft best suited for the application. By making the right choice, you can be sure that the machine will operate efficiently and achieve the desired results.

5 Minutes read

Chains and sprockets: How they work together

Chains and sprockets are important elements in the design and mechanisms of machines and equipment. They are indispensable when it comes to the mechanical transfer of motion and force. But what types of chains and sprockets are there and what are their specific characteristics?

9 Minutes read

Testing technology - Testing of printed circuit boards (spring contact pins)

Reliable test methods are essential in electronics manufacturing. Spring contact pins serve as a precise interface for testing connections in electronic assemblies. But how exactly are spring contact pins used and which variants are available? In this article, you'll discover the many uses and different designs of these precise testing tools.

8 Minutes read

Conveyor technology - Specifications and selection of conveyor timing belts

Conveyor timing belts are a particularly efficient and versatile drive solution in conveyor technology. Unlike conventional conveyor belts or chain drives, they offer synchronized and therefore slip-free power transmission. They are indispensable in many applications. However, there are a few factors to consider when selecting.

7 Minutes read

Pneumatics - Selecting a compact air cylinder in 6 steps

Pneumatic cylinders are versatile drive elements that produce precise linear motion by using compressed air. Depending on the application, different technical properties are required. For example, vacuum valves with volumetric flow restrictors enable precise control of airflow, while integrated anti-rotation devices increase operational reliability. But how do I choose the right compressed air cylinder for my application? This article gives you a comprehensive overview of what is involved when selecting pneumatic cylinders or compressed air cylinders so that you can make informed decisions in the future and select the cylinder that best suits your needs.

12 Minutes read

Cooling and cleaning in production - Air nozzles and spray nozzles

From machining, to welding processes or along the conveyor: In modern manufacturing, precise cooling and reliable cleaning are essential for quality, process reliability and productivity. Air nozzles and spray nozzles offer flexible solutions - from precise blow-off to liquid surface wetting. In this blog, you will learn which nozzle types are suited for which applications, how jet shape and spray angle impact the effect and what really matters when selecting, designing and integrating into the system.

12 Minutes read